This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28335: MPPT tracking problem

Part Number: TMS320F28335

Tool/software: Code Composer Studio

Dear Sir,

I am using MPPT Pno algorithm from the solar library. It is always giving the same voltage values reference value it is not changing. I used the library as the following.

Step 1:  Before the main program, I have included 

#include "Solar_F.h"

MPPT_PNO_F mppt_pno1;

Step 2: In the main program 

MPPT_PNO_F_init(&mppt_pno1);

mppt_pno1.DeltaPmin = 0.0001;
mppt_pno1.MaxVolt = 0.9;
mppt_pno1.MinVolt = 0.65;
mppt_pno1.Stepsize = 0.005;//0.008prev

Step3: Fro every 200 us I am calling the following

mppt_pno1.Ipv = ipavg*0.3333f; // Normalized Panel Current since ISC is 2.9A
mppt_pno1.Vpv = vpavg*0.0492610f; // Normalized Panel Voltage since VOC is 20.3V
// Invoking the MPPT computation macro
MPPT_PNO_F_FUNC(&mppt_pno1);
// Output of the MPPT macro can be written to the reference
// of the voltage regulator
pnew=vpavg*ipavg;
delp=pnew-pold;
if (abs(delp)>1.0f){
mppt_pno1.Stepsize = 0.1;//0.008prev
}else{
mppt_pno1.Stepsize = 0.005;//0.008prev
}
Vpvref_mpptOut = (float32)(mppt_pno1.VmppOut);
vpvref=Vpvref_mpptOut*vbase;
if (vpvref<13.195f){
vpvref=13.195f;
}else if (vpvref>18.27f){
vpvref=18.27f;
}
VPV[ConversionCount]=vpvref;

I tied to debug whether the MPPT_PNO_F.c file is executing or not. I kept the dot in line 37 and 43 to see whether it is executing or not. But it is not pausing the program. 

Please help me in this regard.