Part Number: TMS320F28069M
Dear team:
I use 28069M+drv8301 to control BR2804-1700Kv-1 three phase BLDC motor. Can I modify the program in lab05b to achieve the following functions:
1, The motor will automatically start by 10 sec later after power-on, The initial velocity is 2000rpm.
2, After running for 10 seconds, the speed was adjusted to 4000rpm.
3, After another 10 seconds of operation, the speed was adjusted to 6000 rpm.
4, Run for another 10 seconds to stop the motor, and then repeat the process.
Best regards
- Three phase BLDC motor