This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: EMIF Pin Muxing

Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: C2000WARE

Hi,

I'm planning on making some audio signal processing related projects with my Launchpad the next summer vacancies, so I went exploring C2000Ware files for the TI design of EMIF Board and discovered it uses some high density connector which is not available in my country.

I plan on making a PCB with a 16Mx16 SDRAM to interface with the uC. Is there some way to mux all the EMIF pins to the boosterpack headers pins I have available in my board?

  • Matheus,

    unfortunately all of the signals do not come through the LaunchPad connectors.

    The part number of the High Density connector is DF40C-60DP-0.4V(51). The mating connector that you would need to pun on another board would be DF40C-60DS-0.4V(51).

    Looking at Digi-Key I think both are available to ship to Brazil. Although the estimated shipping cost I saw was ~40 times more than the cost of the component. I suspect that you should be able to find a local distributed that will ship the component for less.

    Hope it helps,
    Cody