Part Number: TIDM-1000
Hello Manish,
I decided to simulate the TIDM in PSIM.
For the simulation, I don't have to worry about feedback offsets because:
1. I assume all feedbacks are perfect (no op-amp offsets and etc.)
2. I don't have to worry about unipolar ADCs, e.g. I compute the voltage and current ADC input value as (Actual Voltage or Current * feedback gain) and then digitize the value between -2048 and 2047.
Could you please verify the feedback gains (shown below) I am using in the simulation.
Thanks,
Stephen
Current Feedback gain:
Current sensor Gain = (4.5V-2.5V)/19.2A
Op-amp gain = 330k/499k
Total Current Feedback gain = Current sensor Gain * Op-amp gain = 0.068887776
Input Voltage Feedback Gain:
ADC Input Voltage at 416.917V Input Voltage = 1.65V
So, Input Voltage Feedback gain = 1.65/416.917 = 0.00395762226
DC Bus Voltage Feedback Gain:
ADC Input Voltage at 454V DC Bus Voltage = 1.67V
So, DC Bus Voltage Feedback gain = 1.67/454 = 0.00367841409
Is 454V the total DC Bus Voltage (Postiive + Negative DC Bus Voltage)?