This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SM320F28335-EP: Aerospace DO254 certification support

Part Number: SM320F28335-EP


Hello
We are evaluating to use the SM320F28335 in an our new project in aerospace field. The device will be cetified according DO254 DAL A.
Can you provide a specific certification package for DO-254 (for DAL A application) for this microcontroller?
Or in alternative can you provide information about:
a. developpement process,
b. life cycle data,
c. functionnal robustness verification performed at isolated IP level,
d. unused functions ( if any ) and what ensures they are disabled.
e. "in service experience" information about ARM based microcontroler used in a safety critical applications
f. feedback about avionic product certification based on this microcontroller
Thank you

  • Nicola,

    We do not support DO-254 with certification package.

    There is some additional information on device use history.  However, this information is NDA only.   I will need to check on if this data is available, and if an NDA can be pursued.

    I will follow up on this via email with you.

    Please  click "This Resolved My Issue" to close out this post.


    Regards,
    Wade