Part Number: TMDSDOCK28379D
Hello,
The schematic of the docking station (TMDSCNCD28377D_180cCARD_pinout_R1_3) says PIN 13 and 29 are ground connected and PIN 16 is connected to +5V supply. However when I did a connectivity test on the hardware I found that these three pins are not connected to the correct terminals (not sure what they are actually connected to). Rest of the pin connections are fine. Can somebody explain this or am I missing something here?
Thanks