This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TIDM-1000: BusMeasCalibrationRoutine.xls is missing

Guru 20075 points

Part Number: TIDM-1000
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE

Tool/software: Code Composer Studio

Hello,

BusMeasCalibrationRoutine.xls is not located in the directory specified in tiducj0a.pdf, i.e. controlSUITE\development_kits\tidm_1000\<version>\hardware\<revision>\

My Control Suite installation doesn't have a <revision> directory in the hardware directory.

The hardware directory has the following two directories:

magnetics_datasheet

MCU011E2

Also, the controlSUITE\development_kits\tidm_1000\v1_01_00_00\docs folder only has the following two files: calculation.xlsx and tiducj0a.pdf

Where can I get the BusMeasCalibrationRoutine.xls file?

Stephen

  • Stephen,

    We have migrated the support for our digital power TIDMs to the Digital Power SDK This will install the C2000Ware base package as well.  I suspect the XLS may be a newer addition and that is why you aren't seeing it in ControlSUITE.

    Let me know if the above package has the XLS you need.

    Best,

    Matthew