Part Number: TMS320F28335
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hi.
I am working on a project where I need to generate a 9 MHz square wave from the f28335 controlCARD. I am unable to do this by simply toggling the GPIOs at 9 MHz speed because it is maxing out at ~3.4 MHz. Going through some of the other threads I discovered that a square wave can be generated up to 25 MHz using the epwm feature of the MCU. I want to ask how do I go about doing this. I am looking through the data sheet but I am having some trouble figuring out the configuration for a 9MHz square wave with a 50% duty cycle. Any suggestion would be much appreciated. Thank you.
Tolu.