Evaluation board: drv8301-hc-evm revd
Lab 10a Overmodulation
Nominal voltage V 24
No load speed rpm 60800
No load current mA 282
Nominal speed rpm 57500
Nominal torque (max. continuous torque) mNm 23.6
Nominal current (max. continuous current) A 6.45
Stall torque mNm 561
Stall current A 149
Max. efciency % 91.6
Terminal resistance W 0.161
Terminal inductance mH 0.0171
Torque constant mNm/A 3.76
Speed constant rpm/V 2540
Speed/torque gradient rpm/mNm 109
Mechanical time constant ms 2.04
Rotor inertia gcm 1.79
when 400rpm,the motor output torque is 70mNm。
I set the maximum current limit of the motor to 60mNm, which confirms that the motor can output 70mNm of torque,
but I use 50mNm of load to jam the motor shaft, the motor occasionally can not start, according to the theory,
the motor 60mNm of torque can completely overcome the 50mNm of load, but in the instant of starting,
the motor stopped without a moment of force, it should be. How to solve the occasional failure of startup in this situation?
The working speed of the motor is 400 rpm