This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-HV-1PH-DCAC: 48VDC Input inverter solution for UPS

Part Number: TIDM-HV-1PH-DCAC

Hi Team,

I'm just looking for a solution for 48V to 100VAC inverter solution for UPS and reached out TIDM-HV-1PH-DCAC which support VSI mode.

But its recommended input voltage was too high(400VDC) as I expected and I'm not sure if we can utilize it as 48V to 100VAC inverter.

Then could you answer following my questions.

1. Is it possible to use this design as 48V to 100VAC inverter?  Let me know if I need other optional board for the use case.

2. Do you have another recommended design for such the use case?

Regards,

Takashi Onawa