This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SM320F28335-HT: McBSP clock and frame sync direction

Part Number: SM320F28335-HT
Other Parts Discussed in Thread: ADS1278

Hi There

In my application we used some reference code to create a McBSP interface to connect to an ADC (ADS1278), This is all now working, but I've just noticed we're using the F28335 MCLKRA and MFSRA pins (ie the receive pins on the master). 

app note SPRUG80A page 19 has the same description for both the transmit and revive clocks "(Supplying or reflecting the receive clock; supplying the input clock of the sample rate generator)"

If they can be both transmit and receive i'm unsure on why they have different labels?

could you confirm there are no issues in using the McBSP clock and frame sync receive pins as a mater transmit?

Kind Regards

Martin