Part Number: TMS320F2808
Hi expert,
How can I get the time from F2808 power up to first running ROM code and the time from start running ROM code to get to main()?
Do you have any existing data for this?
Thanks
Sheldon
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F2808
Hi expert,
How can I get the time from F2808 power up to first running ROM code and the time from start running ROM code to get to main()?
Do you have any existing data for this?
Thanks
Sheldon
Sheldon,
Please refer to the "Power Sequencing" section in the data manual. The Power-on-Reset timing diagram shows when the ROM is executed and the boot mode is read and the transfer is made to the user-code.
Note there is c-setup code that has to be executed before main() which will be dependent on the project itself. The customer will have to measure the time it takes from transfer out of the boot ROM to main().
Regards
Lori