This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28075: TMS320F28075 pwm module minimal impulse

Part Number: TMS320F28075

Good day!

The following, the pulses that form my controller, are physically limited to dead time and are simply skipped when forming low voltages.
Can you please tell the ePWM module the hardware to set the minimum impulse that can be generated by the inverter or less, than it will issue the output fixed filling? or it is completely software task.
Minimum impulse limit code.
Currently, I have 2 pulses when it is filled, and maybe you have a driver that assumes the deadline at the level of the calculation of the filling (not by current feedback).