Part Number: TMDSCNCD28M36
Tool/software: TI-RTOS
Hi i'm using TMDSCNCD28M36 but i cant connect target by an error about XDS100v3.
the code is down.
Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
(Emulation package 8.2.0.00004)
i have controlsuit4.9 installed already and using ccs_v9
and i using xds100v3 usbdebugprobe is my connect setting
let me know what do i need i to do