Part Number: TMS320C28346
Hi Team,
My customer want to use TI C28346 to connect one parallel NOR Flash (1 M x 16bits), one parallel SRAM (1 M x 16bits) and internally set McBSP-A inputs in DMA mode. they plan to use XINTF Zone6 (XZCS6/) for parallel NOR Flash (boot-mode), XINTF zone 7 (XZCS7/) for SRAM. XITNF0 Zone 0 (XZCS0/) for McBSP DMA inputs, is it ok to do this configuration?
I see from the TRM that each XINTF zone on 2834x device can be individually configured with unique read and write access timing and each has an associated zone chip-select signal. This chip-select signal is pulled low so that an access to that zone is currently taking place. On 2834x device, all zone chip select signals are independent.
but I am not sure whether XITNF0 Zone 0 can be use for McBSP-A DMA inputs.