Part Number: TMS320C28346
Hi Team,
From TMS320x2834x Delfino Boot ROM Reference Guide, it list the part of SPI EEPROM as below which all are very small, question is if SPI boot can support 512KB or bigger SPI EEPROM or flash? any suggestion about this type of device which is not limited to Atmel?
The SPI boot ROM loader initializes the SPI module to interface to a serial SPI EEPROM or flash. Devices
of this type include, but are not limited to, the Xicor X25320 (4Kx8) and Xicor X25256 (32Kx8) SPI serial
SPI EEPROMs and the Atmel AT25F1024A serial flash.