Part Number: TMS320F28035
Customer wants to use AIO function due to limited GPIO amount with F28035. There is one statement in the datasheet:
Unused ADCIN pins that are multiplexed with AIO function should not be directly connected to analog ground. They should be grounded through a 1-kΩ resistor. This is to prevent an errant code from configuring these pins as AIO outputs and driving grounded pins to a logic-high state.
Could you give some suggestion on the hardware design if using AIO function for input or output? As we know, it might impact the performance of the analog peripherals due to noise coupling. Thank you.