This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: Slow response CMPSS

Part Number: TMS320F280049


SIr/Madam,

I have used cmpss module to trigger tripzone in epwm using epwm crossbar.

For that following setting I have done.

    AnalogSubsysRegs.CMPHPMXSEL.bit.CMP1HPMXSEL = 1;//O/C-N
     Cmpss1Regs.COMPCTL.bit.COMPHSOURCE         = NEGIN_DAC;
     Cmpss1Regs.COMPDACCTL.bit.SELREF           = REFERENCE_VDDA;
     Cmpss1Regs.DACHVALS.bit.DACVAL             = 1862;//  1.5V
     Cmpss1Regs.CTRIPHFILCLKCTL.bit.CLKPRESCALE = 100;
     Cmpss1Regs.CTRIPHFILCTL.bit.SAMPWIN        = 0x1F;
     Cmpss1Regs.CTRIPHFILCTL.bit.THRESH         = 30;    //3us
     Cmpss1Regs.CTRIPHFILCTL.bit.FILINIT        = 1;
     Cmpss1Regs.COMPCTL.bit.CTRIPHSEL           = CTRIP_FILTER;
     Cmpss1Regs.COMPCTL.bit.CTRIPOUTHSEL        = CTRIP_FILTER;

    EPwm1Regs.TZDCSEL.bit.DCBEVT1          = TZ_DCBH_HI;//0x2
    EPwm1Regs.DCTRIPSEL.bit.DCBHCOMPSEL    = 0xF; //DCBHTRIPSEL
    EPwm1Regs.TZSEL.bit.DCBEVT1            = 1;
    EPwm1Regs.DCBCTL.bit.EVT1SRCSEL        = DC_EVT1;
    EPwm1Regs.DCBCTL.bit.EVT1FRCSYNCSEL    = DC_EVT_ASYNC;
    EPwm1Regs.DCBHTRIPSEL.bit.TRIPINPUT7   = 1;
    EPwmXbarRegs.TRIP7MUX0TO15CFG.bit.MUX0 = 0;
    EPwmXbarRegs.TRIP7MUXENABLE.bit.MUX0   = 1;

    EPwm1Regs.TZCLR.bit.OST = 1;
    EPwm1Regs.TZCLR.bit.CBC = 0;
    EPwm1Regs.TZCLR.bit.INT = 1;

System clock = 100Mhz

Now when I give slowly rising signal on comparator input, the trip is delayed by 18 milliseconds. And when I give relatively fast signal trip gets delayed only by 56 microseconds.

For your reference i am attaching following images.

Channel A: comparator input

Channel B: Tripzone interrup


When comparator input is changed fast, tripzone gets triggered instantly.

While levels have been set same at 1.5V in both cases.


Channel B: input of comparator

So please tell why this comparator output is delayed by such long time?

Thanks

Rishabh