Part Number: TIDM-1003
Hello,
Im having difficulties with finding the proper programmator and the proper adapter for programming the mentioned TIDM-1003?
So I've made a PCB according to your provided gerber files. Then I've bought an original XDS100V2 JTag emulator with 14-Pin JTAG Header.
Now, according to the TIDM-1003 schematics and according to the pinout of the 14 pin JTAG header, it's not matched. I dont want to manually solder wires and connecting them to the emulator, I'd like to have some sort of an adaptor so I could have connection between TIDM-1003 and XDS100V2.
If anyobody has any experience with programming TIDM-1003 via JTAG, I would be very grateful if he/she could share some info, especially on which emulator and which adapter to use, and how to connect them.
The connections for JTAG on TIDM-1003 are on J9, and are as follows:
TDI -- 1 2 -- NC
NC -- 3 4 -- TMS
TDO -- 5 6 -- NC
NC -- 7 8 -- TCLK
nRST -- 9 10 -- TMS
NC -- 11 12 -- VCC
GND -- 13 14 -- NC
Thanks in advance,
Mitja