Part Number: TMS320F28379S
Other Parts Discussed in Thread: C2000WARE
Dear Sir ,
We are developing our product based on 283376S Chip , we are using several ePWMs channels separately (e.g Channel A for Output 1 , channel B for Output 2 )
the complementary and dead time is done by hardware.
we mange to work the ePWM as we interned at 20Khz from Sysclk of 200Mhz , the PMW is symmetric around its mid point (e.g. PWM in Up - Dowm mode) , and we wish to work in high resolution
mode.
we have tried various example and read some post regarding high resolution duty cycle in symmetric PMW , such as the post below
http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/698811?CCS-TMS320F28035-HRPWM-for-for-hi-res-duty-control-in-up-down-count-symmetric-mode
and came to conclusion (maybe we are doing something wrong) that for high resolution duty cycle cannot be achieved only by MEP as it only delay the edge of the PMW and thus can not be symmetric (because for symmetric it need to move the edges in opposite direction e.g delay the rising edge and precede the falling edge )
1. please clarify this issue
2.if you have example for duty cycle control in high resolution PWM (symmetric ) , please provide