Part Number: TMS320F28379D
Other Parts Discussed in Thread: CDCLVC1102
Tool/software: Code Composer Studio
Hi,
The TIDA-01455 document explains as "The design features an interface to the C2000™ Delfino™ to generate up to a 20-MHz clock signal and receive and decode the modulated bit stream from the AMC1306 in Manchester coded bit format."
As I check the schematic of TIDA-01455, the CLKIN is provided by CDCLVC1102.
Is it possible to provide CLKIN from F28379D? (Is the MCLK from F28379D useful for CLKIN?)
Regards,
Nagata.