Other Parts Discussed in Thread: TI-CGT, CONTROLSUITE
Tool/software: Code Composer Studio
Hi,
I'm also using Simulink to builld code for the LAUNXL - F2839D Eval Kit. On my Windows 7 Laptop everythin works fine. But the Build Process takes very long time, so i wanted to do it with the worksation. There ist Windows 10 installed. The code configuration options are the same but at the workstation i get the following error report:
<### Creating CCS Project at : C:\Users\KaRaT\Documents\MATLAB\Induktiv\TI_Controller_ert_rtw\CCS_Project ### CCS project created successfully Open project in Code Composer Studio.
### Using toolchain: Texas Instruments C2000 Code Generation Tools v16.9.2 | gmake (64-bit Windows) ### 'C:\Users\KaRaT\Documents\MATLAB\Induktiv\TI_Controller_ert_rtw\TI_Controller.mk' is up to date ### Building 'TI_Controller': "D:\Program Files\Mathworks\bin\win64\gmake" MATLAB_ROOT=%MATLAB_ROOT% ALT_MATLAB_ROOT=%ALT_MATLAB_ROOT% MATLAB_BIN=%MATLAB_BIN% ALT_MATLAB_BIN=%ALT_MATLAB_BIN% -B -f TI_Controller.mk all C:\Users\KaRaT\Documents\MATLAB\Induktiv\TI_Controller_ert_rtw>call "\\DESKTOP-457H9UG\D$\Program Files\Mathworks\bin\win64\checkMATLABRootForDriveMap.exe" "\\DESKTOP-457H9UG\D$\Program Files\Mathworks" 1>mlEnv.txt C:\Users\KaRaT\Documents\MATLAB\Induktiv\TI_Controller_ert_rtw>for /F %a in (mlEnv.txt) do set "%a"\n C:\Users\KaRaT\Documents\MATLAB\Induktiv\TI_Controller_ert_rtw>set "MATLAB_ROOT=F:"\n C:\Users\KaRaT\Documents\MATLAB\Induktiv\TI_Controller_ert_rtw>set "ALT_MATLAB_ROOT=F:"\n C:\Users\KaRaT\Documents\MATLAB\Induktiv\TI_Controller_ert_rtw>set "MATLAB_BIN=F:\bin"\n C:\Users\KaRaT\Documents\MATLAB\Induktiv\TI_Controller_ert_rtw>set "ALT_MATLAB_BIN=F:\bin"\n C:\Users\KaRaT\Documents\MATLAB\Induktiv\TI_Controller_ert_rtw>cd . C:\Users\KaRaT\Documents\MATLAB\Induktiv\TI_Controller_ert_rtw>if "" == "" ("D:\Program Files\Mathworks\bin\win64\gmake" MATLAB_ROOT=F: ALT_MATLAB_ROOT=F: MATLAB_BIN=F:\bin ALT_MATLAB_BIN=F:\bin -B -f TI_Controller.mk all ) else ("D:\Program Files\Mathworks\bin\win64\gmake" MATLAB_ROOT=F: ALT_MATLAB_ROOT=F: MATLAB_BIN=F:\bin ALT_MATLAB_BIN=F:\bin -B -f TI_Controller.mk ) C:/PROGRA~3/MATLAB/SUPPOR~1/R2018b/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2018b/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=TI_Controller -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DTID01EQ=0 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=512 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=TI_Controller -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -IC:/Users/KaRaT/Documents/MATLAB/Induktiv -IC:/Users/KaRaT/Documents/MATLAB/Induktiv/TI_Controller_ert_rtw -IC:/Users/KaRaT/Documents/MATLAB/InduktivesLaden -IF:/extern/include -IF:/simulink/include -IF:/rtw/c/src -IF:/rtw/c/src/ext_mode/common -IF:/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2018b/toolbox/target/SUPPOR~1/tic2000/inc -IF:/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2018b/toolbox/target/SUPPOR~1/tic2000/src -ID:/Program Files/TI/ControlSuite/device_support/F2837xD/v190/F2837xD_common/include -ID:/Program Files/TI/ControlSuite/device_support/F2837xD/v190/F2837xD_headers/include -ID:/Program Files/TI/ControlSuite/device_support/F2837xD/v190/F2837xD_common -IF:/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2018b/toolbox/target/shared/EXTERN~1/include --output_file=MW_c28xx_board.obj MW_c28xx_board.c [include.] >> WARNING: more than one source file is specified; option --output_file is ignored Fatal error: cannot open source file "Files/TI/ControlSuite/device_support/F2837xD/v190/F2837xD_common/include" 1 catastrophic error detected in the compilation of "Files/TI/ControlSuite/device_support/F2837xD/v190/F2837xD_common/include". Compilation terminated. >> Compilation failure gmake: *** [MW_c28xx_board.obj] Error 1 C:\Users\KaRaT\Documents\MATLAB\Induktiv\TI_Controller_ert_rtw>echo The make command returned an error of 2 The make command returned an error of 2 C:\Users\KaRaT\Documents\MATLAB\Induktiv\TI_Controller_ert_rtw>An_error_occurred_during_the_call_to_make Der Befehl "An_error_occurred_during_the_call_to_make" ist entweder falsch geschrieben oder konnte nicht gefunden werden. ### Creating HTML report file TI_Controller_codegen_rpt.html
### Build procedure for model: 'TI_Controller' aborted due to an error.
Error(s) encountered while building "TI_Controller": ### Failed to generate all binary outputs.
Component:Simulink | Category:Block diagram error
/>
/>