Other Parts Discussed in Thread: DRV8312, DRV8301, CONTROLSUITE, DRV8303EVM, TMS320F28035
1. I want to make a motor control scheme with hall sensor. The speed can be controlled in a closed loop.
Even if I apply a load, the motor speed will not drop, or the speed can be quickly restored to the set speed after falling.
(Voltage 30V, current 15A,Hall)
DRV8312-C2-KIT:DRV8312 three phase inverter baseboard + Piccolo TMDSCNCD28035MISO controlCARD
BLDC_Sensored is what I need,but max_current 3.5A,
DRV8301-HC-C2-KIT:DRV8301 three phase inverter baseboard + Piccolo TMDSCNCD28035MISO controlCARD
Sensorless 60A,There is no BLDC_Sensored software code,
How to transplant BLDC_Sensored software code from DRV8312-C2-KIT to DRV8301-HC-C2-KIT?
2.How to transplant HVBLDC_Sensored software code from HVMotorCtrl+PfcKit_v2.0 to DRV8301-HC-C2-KIT?