Part Number: TMDSHVMTRINSPIN
Other Parts Discussed in Thread: TMS320F28027F, TMDSCNCD28035
Dear TI Experts:
Today I first tried TMDSHVMTRINSPIN kit. I use AC110V and 15VDC (aux power) with [M3]-J5 populated and [Main]-J9 removed (F28069M controlCARD is used). Also, a banana line from BS1 to BS5, and J2, J3, J4, J5, J7, and J8 all follows the instructions in the document.
For the F28069M controlCARD, I set
SW1: UP-UP
SW2: DOWN-DOWN
SW3: UP-UP
Finally, I connect F28069M controlCARD with my computer, and run the related GUI program, and get the following error message.
In fact, in the beginning I set SW3: DOWN-DOWN by reading a Boot Modes table. But it shows the same result. I entered the GUI system, used its connection wizard, and the connection still failed!
Finally, I changed the card as the Piccolo TMS320F28027F non-isolated controlCARD with [M3]-J5 removed and [Main]-J9 populated. Then I run another GUI program, and connection still fail, as shown below.
I have tried many times. I really hope the experienced experts can guide me to continue it. Mant thanks!
Best Wishes,
Tang Han.