Other Parts Discussed in Thread: C2000WARE
Hi Team,
My customer are using USB function of TMS320F28377S and verify this function ok in his computer, when they connected usb port on TMS320F28377S to some of other computer, there will have an issue that unable to install the usb driver, they try to install the driver from the below folder in C2000ware, but it show "system can not find target file" as below showed in Chinese.
Customer try many computers, only 20% has no issue, is there any suggestion to help fix this issue for the rest of 80% computer?
C:\ti\c2000\C2000Ware_2_00_00_02\utilities\flash_programmers\usb_flash_programmer\windows_driver