Other Parts Discussed in Thread: CONTROLSUITE, INSTASPIN-BLDC
1.Does Instaspin BLDC have detailed user guides like instaspin-foc and instaspin-motion user guides?
How come it's all about how that GUI is used, there's no documentation like instaspin-foc on program structure?
2.I use Evaluation board: drv8301-hc-evm revd Lab 10a Overmodulation realize low speed and high torque function of brushless dc motor,
Nominal voltage V 24
No load speed rpm 60800
No load current mA 282
Nominal speed rpm 57500
Nominal torque (max. continuous torque) mNm 23.6
Nominal current (max. continuous current) A 6.45
when 300rpm,the motor output torque is 70mNm,
I use Instaspin BLDC Whether the brushless dc motor can also achieve low speed high torque function?