This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F280049C: Launchpad for Instaspin

Part Number: LAUNCHXL-F280049C


Hello Ti,

I am writing, because I want to use Instaspin-FOC with my own hardware. In the past I used the F28069m with the DRV8301-H2-Kit, but then I saw that the new Launchpad F280049c is also capable of Instaspin.

I’ve checked out the Instaspin Solution for the F280049c and it looks a bit different from the Instaspin used for the F28049m.

What are the main differences?

On a different note, which MCU should I use: the 049c or the 069m? Are there any advantages or disadvantages regarding one or the other?

 

Thanks in advance