Part Number: TMS320F28335
Tool/software: Code Composer Studio
Hi all,
I am trying to connect an SD card with my DSP and I am trying to follow the famous spraao7 guide. I am stuck at including the "DSP280x_Device_lib.h" file.
It seems that this file has been developed for 280x devices, whereas I am using 28335. Do I need to make some changes in this file? The code for this file is listed below:
// TI File $Revision: /main/4 $
// Checkin $Date: August 2, 2006 16:58:50 $
//###########################################################################
//
// FILE: DSP280x_Device.h
//
// TITLE: DSP280x Device Definitions.
//
//###########################################################################
// $TI Release: DSP280x, DSP2801x Header Files V1.41 $
// $Release Date: August 7th, 2006 $
//###########################################################################
#ifndef DSP280x_DEVICE_H
#define DSP280x_DEVICE_H
#ifdef __cplusplus
extern "C" {
#endif
#define TARGET 1
//---------------------------------------------------------------------------
// User To Select Target Device:
#define DSP28_28015 0
#define DSP28_28016 0
#define DSP28_2809 0
#define DSP28_2808 TARGET
#define DSP28_2806 0
#define DSP28_2802 0
#define DSP28_2801 0
//---------------------------------------------------------------------------
// Common CPU Definitions:
//
extern cregister volatile unsigned int IFR;
extern cregister volatile unsigned int IER;
#define EINT asm(" clrc INTM")
#define DINT asm(" setc INTM")
#define ERTM asm(" clrc DBGM")
#define DRTM asm(" setc DBGM")
#define EALLOW asm(" EALLOW")
#define EDIS asm(" EDIS")
#define ESTOP0 asm(" ESTOP0")
#define M_INT1 0x0001
#define M_INT2 0x0002
#define M_INT3 0x0004
#define M_INT4 0x0008
#define M_INT5 0x0010
#define M_INT6 0x0020
#define M_INT7 0x0040
#define M_INT8 0x0080
#define M_INT9 0x0100
#define M_INT10 0x0200
#define M_INT11 0x0400
#define M_INT12 0x0800
#define M_INT13 0x1000
#define M_INT14 0x2000
#define M_DLOG 0x4000
#define M_RTOS 0x8000
#define BIT0 0x0001
#define BIT1 0x0002
#define BIT2 0x0004
#define BIT3 0x0008
#define BIT4 0x0010
#define BIT5 0x0020
#define BIT6 0x0040
#define BIT7 0x0080
#define BIT8 0x0100
#define BIT9 0x0200
#define BIT10 0x0400
#define BIT11 0x0800
#define BIT12 0x1000
#define BIT13 0x2000
#define BIT14 0x4000
#define BIT15 0x8000
//---------------------------------------------------------------------------
// For Portability, User Is Recommended To Use Following Data Type Size
// Definitions For 16-bit and 32-Bit Signed/Unsigned Integers:
//
#ifndef DSP28_DATA_TYPES
#define DSP28_DATA_TYPES
typedef int int16;
typedef long int32;
typedef unsigned int Uint16;
typedef unsigned long Uint32;
typedef float float32;
typedef long double float64;
#endif
//---------------------------------------------------------------------------
// Include Peripheral Header Files:
//
#include "DSP2833x_Gpio.h" // General Purpose I/O Registers
#include "DSP2833x_Spi.h" // SPI Registers
#ifdef __cplusplus
}
#endif /* extern "C" */
#endif // end of DSP280x_DEVICE_H definition
//===========================================================================
// End of file.
//===========================================================================
Regards,