Per TMS320f2837x TRM the reset entry point is configurable to either Flash - 0x080000 or RAM - 0x000000. I'm wondering if I configure reset entry point as RAM - 0x000000 then, after reset how the executable code will be available at this location. As the RAM is non-volatile memory after reset the data will be lost. can someone explain this RAM reset entry point scenario?