Part Number: TMDSSOLARPEXPKIT
Tool/software: Code Composer Studio
Hello I am working with TMDSSOLARPEXPKIT, but I want to use version v1.2 instead of v1.0. I add files to includes folder and initialize macro, but I receive errror like this:
"../F28035_FLASH_SolarExplorer.CMD", line 116: error: program will not fit into
available memory. placement with alignment/blocking fails for section
".econst" size 0x21 page 0. Available memory ranges:
FLASHA size: 0x1f80 unused: 0x5 max hole: 0x4
"../F28035_FLASH_SolarExplorer.CMD", line 120: error: program will not fit into
available memory. placement with alignment/blocking fails for section
"IQmath" size 0x15d page 0. Available memory ranges:
FLASHA size: 0x1f80 unused: 0x5 max hole: 0x4
error: errors encountered during linking; "SolarExplorer_PVInverter.out" not
built