Part Number: TMDSEMU110-U
Hello Team,
My customer is facing a problem of noised ground while connecting XDS110 to his PCB and the PC.
Brief description of the problem below:
All the voltages in the PCB are the same polluted during connection of XDS110 to the PCB. There is some random noise appears on the power.
The amplitude of such noise is approximately about 50mv peak. Actually, XDS110 gets its power from my PCB (please see attached adapter card)
Ones I have several references on my PCB they are all affected by this fluctuation resulting in incorrect analog measurements (in my case it is current).
Then the XDS110 is connected only to power (via phone adapter for example) this problem does not exist, only if XDS110 is connected to the Laptop (even no communication presents from the DSP side)
I use Matlab and Simulink and communicate to the target via External Mode for the debugging, so in this situation, the XDS110 is connected to the target and communicate instantly, but the reading of the analog measurements is wrong and noisy ( I verified it by scope measurement in the hardware) in this situation. The distance (harness length) between the target and the XDS110 is about 30 cm. I use buffer to compensate the length (see attached)
Does all inputs/outputs from the target side of the debugger and target power are optically isolated (like in XDS100)? Can I get the internal Elec. Schematic of the debugger to see that I can do in order to solve this problem or please provide your solution.
ADAPTER FOR JTAG COMM _ JTAG_.pdf
Please advise the above, thank you very much.
Best regards,
Shai