Part Number: TIDM-HV-1PH-DCAC
I am using this module in grid connected mode, without any modifications to the hardware or software. Build 1 and Build 2: DC Check work just fine. When I move to Build 2: AC Check, I connect the relays, but whenever I select rlyConnect to 1, it immediately goes into Overcurrent trip mode and the relays switch off. This happens no matter if invloRef is set to 0.01 or 0, and with a DC Bus Voltage of 300 V. I don't have access to an AC power supply so I'm just plugging the AC side directly into an outlet. Do you have any advice?
Thank you!