Other Parts Discussed in Thread: C2000WARE
Hi,
We have a launchpad with TMS320F28379D controller. I have configured the PLL and wanted to check the clock frequency on XCLKOUT/GPIO73. As per the schematics in SPRUI77C, page 16, GPIO73 is available on J9 connector at pin 37. But when I configured the GPIO as XCLKOUT and probed on the Oscilloscope, I did not see any waveform. It was just a continuous low.
After that, I randomly changed the pull up disable (GPCPUD) registers for different pins and found that pin 37 of J9 connector is actually to connected to GPIO70 instead of GPIO73.
Then I thought I might have gone wrong with the pin counts. Since as per the schematics, pin 1 is ground, I thought of finding out pin 1 on the board using DMM. But I found that none of the corner pins are ground. This makes me believe that the schematics of this launchpad is a whole mess. Could you please help me out on this?
Thank you.
Gobind Singh