This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: LAUNCHXL-F28379D Launchpads erase flash error/cannot be programmed

Part Number: TMS320F28379D
Other Parts Discussed in Thread: LAUNCHXL-F28379D

Hi,

I recently ordered two new LAUNCHXL-F28379D Launchpads and I am not able to program any of these launchpads. The same code when I load to one of the old launchpads (same part number), it flashes without any issues.

I get an error saying verification failed, the code at location 0x080076 does not match with the image. I tried changing the address of the memory to a different one, but that did not help. Below is the memory that we are using.

M1 : origin = 0x080002, length = 0x0020
M2 : origin = 0x080022, length = 0x0052
M3 : origin = 0x080074, length = 0x0002
M4 : origin = 0x080076, length = 0x0100
M5 : origin = 0x080176, length = 0x1000
M6 : origin = 0x081176, length = 0x0080

I also tried to just erase flash without loading program using the CCS option, but it shows the error saying "the controller is either not connected or this operation is not allowed". 

I also checked the boot switches, they all match with the working board. So this should not be the problem.

We are worried that we might have received faulty boards. Could you please put some light on this problem?

We ordered two boards and both of them have this problem.

Thank you.

Gobind Singh