Part Number: TMS320F280049
Other Parts Discussed in Thread: C2000WARE, LAUNCHXL-F280049C
Hello,
I have a question about SPI timing for F280049.
I’m referring to datasheet “TMS320F28004x Piccolo Microcontrollers datasheet RevD” SPRS945D:
Figure 5-74. SPI Master Mode External Timing (Clock Phase = 0)
Figure 5-75. SPI Master Mode External Timing (Clock Phase = 1)
When F28004x SPI is in Master mode, and sending two or more commands back to back, SPISTE will change valid to invalid at the end of the 1st command (*1), and then will change to valid again at the start of the 2nd command soon (*2).
I’m unable to find any specification for the time between *1 and *2 in the datasheet.
Please find below figure for details.
Could you please let me know that information?
Regards,
-Shibata