Part Number: TMS320F280049C
Other Parts Discussed in Thread: C2000WARE
Hi Team,
when connected launchpad F280049c to ccs without load any code, then CMP1HPMXSEL and CMP3HPMXSEL is set to 2 as below showed. which is not matched with datasheet which should be 0 after reset. is anything wrong here?
if load the code from c2000ware as below, it seems there is no function to configure the CMP1HPMXSEL, it is easy to make confusion.
C:\ti\c2000\C2000Ware_2_00_00_02\driverlib\f28004x\examples\cmpss
Also if I change CMP1HPMXSEL to 3 in the ccs windows, then click reset command in ccs, then CMP1HPMXSEL value still remain 3, but other register like Cmpss1Regs will be reset to 0, why CMP1HPMXSEL remain no change?