Part Number: TMS320F28035
As shown in F2803x datasheet, the typical specifications for CL1 and CL2 are 12pF for 20MHz.
There is a note that "CL1 and CL2 are the total capacitance of the circuit board and components excluding the IC and crystal. The value is usually approximately twice the value of the crystal's load capacitance."
So, does it mean that the crystal's load capacitance should be about 6pF? How much should the value of CL1 and CL2 be?
Customer wants to use a crystal with load capacitance CL of 8~12pF. Is it a suitable one?