This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000WARE-DIGITALPOWER-SDK: i can't find an approperiate camera with high resolution that can send live frames to C2000 Delfino MCU F28379D

Part Number: C2000WARE-DIGITALPOWER-SDK


i'm working on a project that is live video conferencing , the hardware is that the camera send the live frames it takes to the C2000 Delfino MCU F28379D instant by instant through uart or I2C protocol and then

the C2000 Delfino MCU F28379D sends that frames to tivaC 1294 and the tivaC 1294 controls (displays)   the    BOOSTXL-K350QVG-S1  

and the BOOSTXL-K350QVG-S1 displays the live stream video i mean with the live stream the camera snaps or frames i don't mean any wifi or ethernet

1)what are the best protocols between devices ?

2) what is the best camera that can do this with the delphino ?

thanks in advance