This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: CAN: Read multiple times from IF3 during one RX interrupt

Part Number: TMS320F280049

Hi,

is it possible to read multiple times from IF3 during one RX interrupt? In my application it is possible, that there are already two message when I get into the RX interrupt for the first time.

I tried to read the IF3Upd-flag in a loop. At the end of each iteration all configured registers in IF3_OBS are read. This does not work. The IF3Upd-flag is only set once.

The next RX interrupt is triggered with the next message.

So I will always read the message before the current and will never get to the current.

What can I do?

Best regards,

Stefan W.