This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28335: Boot-Rom COFF File

Part Number: TMS320F28335
Other Parts Discussed in Thread: C2000WARE

Tool/software: Code Composer Studio

Hi,

I'm working on the boot-rom project. I converted to .out file to coff file via hex2000. Should I directly send bytes in coff files via selected peripheral such as CanBus? I'm using CAN-boot. I parsed coff file as two-byte arrays due to Boot-rom document's explanation. 

The MCU goes in boot mode. It's okay. I tested the boot-mode with CodeSkin Chip Programmer. It's working. But I want to try to send coff file in boot mode with my application. It's not working. How can i use coff file? 

Note: C2Prog is using .out file.

Thank you.