Part Number: UNIFLASH
Other Parts Discussed in Thread: F28M36P63C2
We are using Uniflash to program our F28M36P63C2 device.
We would like to be able to place a small amount (around 8 bytes) of calibration data in a spare bank of the C28 core's flash independently of programming the main application code.
This would need to be at an address that we can define so that the application can access the entered values.
Is this possible? If so, can you give an example of the file format we need to generate, and the Uniflash command line necessary?
Many thanks.