This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: transmit data from scia to scib at same MCU

Part Number: TMS320F28379D


I using f28379d and i want to transmit data from SCIA to SCIB but i get garbage
i using echo_back example from c2000_ware with some edits

//###########################################################################
//
// FILE:    Example_2837xDSci_Echoback.c
//
// TITLE:   SCI Echoback.
//
//! \addtogroup cpu01_example_list
//! <h1>SCI Echoback (sci_echoback)</h1>
//!
//!  This test receives and echo-backs data through the SCI-A port.
//!
//!  The PC application 'hyperterminal' or another terminal
//!  such as 'putty' can be used to view the data from the SCI and
//!  to send information to the SCI.  Characters received
//!  by the SCI port are sent back to the host.
//!
//!  \b Running \b the \b Application
//!  -# Configure hyperterminal or another terminal such as putty:
//!
//!  For hyperterminal you can use the included hyperterminal configuration
//!  file SCI_96.ht.
//!  To load this configuration in hyperterminal
//!    -# Open hyperterminal
//!    -# Go to file->open
//!    -# Browse to the location of the project and
//!       select the SCI_96.ht file.
//!  -# Check the COM port.
//!  The configuration file is currently setup for COM1.
//!  If this is not correct, disconnect (Call->Disconnect)
//!  Open the File-Properties dialogue and select the correct COM port.
//!  -# Connect hyperterminal Call->Call
//!  and then start the 2837xD SCI echoback program execution.
//!  -# The program will print out a greeting and then ask you to
//!  enter a character which it will echo back to hyperterminal.
//!
//!  \note If you are unable to open the .ht file, or you are using
//!  a different terminal, you can open a COM port with the following settings
//!  -  Find correct COM port
//!  -  Bits per second = 9600
//!  -  Date Bits = 8
//!  -  Parity = None
//!  -  Stop Bits = 1
//!  -  Hardware Control = None
//!
//!  \b Watch \b Variables \n
//!  - LoopCount - the number of characters sent
//!
//! \b External \b Connections \n
//!  Connect the SCI-A port to a PC via a transceiver and cable.
//!  - GPIO28 is SCI_A-RXD (Connect to Pin3, PC-TX, of serial DB9 cable)
//!  - GPIO29 is SCI_A-TXD (Connect to Pin2, PC-RX, of serial DB9 cable)
//!
//
//###########################################################################
// $TI Release: F2837xD Support Library v3.06.00.00 $
// $Release Date: Mon May 27 06:48:24 CDT 2019 $
// $Copyright:
// Copyright (C) 2013-2019 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
//   Redistributions of source code must retain the above copyright
//   notice, this list of conditions and the following disclaimer.
//
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the
//   documentation and/or other materials provided with the
//   distribution.
//
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################
//
// Included Files
//
#include "F28x_Project.h"
//
// Globals
//
Uint16 LoopCount;
char x=0;
Uint16 Received[100];
//
// Function Prototypes
//
void scia_echoback_init(void);
void scia_fifo_init(void);
void scia_xmit(int a);
void scia_msg(char *msg);
void scia_rec (void);
//
// Main
//
void main(void)
{
    char *msg;
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2837xD_SysCtrl.c file.
//
   InitSysCtrl();
//
// Step 2. Initialize GPIO:
// This example function is found in the F2837xD_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//
   InitGpio();
//
// For this example, only init the pins for the SCI-A port.
//  GPIO_SetupPinMux() - Sets the GPxMUX1/2 and GPyMUX1/2 register bits
//  GPIO_SetupPinOptions() - Sets the direction and configuration of the GPIOS
// These functions are found in the F2837xD_Gpio.c file.

   GPIO_SetupPinMux(43, GPIO_MUX_CPU1, 0xf);
   GPIO_SetupPinOptions(43, GPIO_INPUT, GPIO_PUSHPULL);
   GPIO_SetupPinMux(42, GPIO_MUX_CPU1, 0xf);
   GPIO_SetupPinOptions(42, GPIO_OUTPUT, GPIO_ASYNC);
   GPIO_SetupPinMux    (19 , GPIO_MUX_CPU1    , 2            ); // set pin 18 to MUX position 2 as UARTA RX
   GPIO_SetupPinOptions(19 , GPIO_INPUT       , GPIO_PUSHPULL); // set pin as RX
   GPIO_SetupPinMux    (18 , GPIO_MUX_CPU1    , 2            ); // set pin 19 to MUX position 2 as UARTA TX
   GPIO_SetupPinOptions(18 , GPIO_OUTPUT      , GPIO_ASYNC   ); // set pin as TX
// Step 3. Clear all __interrupts and initialize PIE vector table:
// Disable CPU __interrupts
//
   DINT;
//
// Initialize PIE control registers to their default state.
// The default state is all PIE __interrupts disabled and flags
// are cleared.
// This function is found in the F2837xD_PieCtrl.c file.
//
   InitPieCtrl();
//
// Disable CPU __interrupts and clear all CPU __interrupt flags:
//
   IER = 0x0000;
   IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the __interrupt
// is not used in this example.  This is useful for debug purposes.
// The shell ISR routines are found in F2837xD_DefaultIsr.c.
// This function is found in F2837xD_PieVect.c.
//
   InitPieVectTable();
//
// Step 4. User specific code:
//
   LoopCount = 0;
   scia_fifo_init();       // Initialize the SCI FIFO
   scia_echoback_init();   // Initialize SCI for echoback
   for(;;)
   {
       msg = "\r\nEnter a character: \0";
       scia_msg(msg);
       //
       // Wait for inc character
       //
       scia_rec();
   }
}
//
//  scia_echoback_init - Test 1,SCIA  DLB, 8-bit word, baud rate 0x000F,
//                       default, 1 STOP bit, no parity
//
void scia_echoback_init()
{
    //
    // Note: Clocks were turned on to the SCIA peripheral
    // in the InitSysCtrl() function
    //
    SciaRegs.SCICCR.all = 0x0007;   // 1 stop bit,  No loopback
                                    // No parity,8 char bits,
                                    // async mode, idle-line protocol
    SciaRegs.SCICTL1.all = 0x0003;  // enable TX, RX, internal SCICLK,
                                    // Disable RX ERR, SLEEP, TXWAKE
    SciaRegs.SCICTL2.all = 0x0003;  //enable TX,RX interrupt
    SciaRegs.SCICTL2.bit.TXINTENA = 1;
    SciaRegs.SCICTL2.bit.RXBKINTENA = 1;

    //
    // SCIA at 9600 baud
    // @LSPCLK = 50 MHz (200 MHz SYSCLK) HBAUD = 0x02 and LBAUD = 0x8B.
    // @LSPCLK = 30 MHz (120 MHz SYSCLK) HBAUD = 0x01 and LBAUD = 0x86.
    //
    SciaRegs.SCIHBAUD.all = 0x0002;
    SciaRegs.SCILBAUD.all = 0x008B;
    SciaRegs.SCICTL1.all = 0x0023;  // Relinquish SCI from Reset

    //
       // Note: Clocks were turned on to the SCIB peripheral
       // in the InitSysCtrl() function
       //
       ScibRegs.SCICCR.all = 0x0007;   // 1 stop bit,  No loopback
                                       // No parity,8 char bits,
                                       // async mode, idle-line protocol
       ScibRegs.SCICTL1.all = 0x0003;  // enable TX, RX, internal SCICLK,
                                       // Disable RX ERR, SLEEP, TXWAKE
       ScibRegs.SCICTL2.all = 0x0003;  //enable TX,RX interrupt
       ScibRegs.SCICTL2.bit.TXINTENA = 1;
       ScibRegs.SCICTL2.bit.RXBKINTENA = 1;
       //
       // SCIB at 9600 baud
       // @LSPCLK = 50 MHz (200 MHz SYSCLK) HBAUD = 0x02 and LBAUD = 0x8B.
       // @LSPCLK = 30 MHz (120 MHz SYSCLK) HBAUD = 0x01 and LBAUD = 0x86.
       //
       ScibRegs.SCIHBAUD.all = 0x0002;
       ScibRegs.SCILBAUD.all = 0x008B;
       ScibRegs.SCICTL1.all = 0x0023;  // Relinquish SCI from Reset
}
//
// scia_xmit - Transmit a character from the SCI
//
void scia_xmit(int a)
{
    while (SciaRegs.SCIFFTX.bit.TXFFST != 0) {}
    SciaRegs.SCITXBUF.all =a;
}
//
// scia_msg - Transmit message via SCIA
//
void scia_msg(char * msg)
{
    int i;
    i = 0;
    while(msg[i] != '\0')
    {
        scia_xmit(msg[i]);
        i++;
        break;
    }
}
void scia_rec (void)
{
    while(ScibRegs.SCIFFRX.bit.RXFFST == 0) { } // wait for empty state
    //
    // Get character
    //
    Received[x] = ScibRegs.SCIRXBUF.all;
    x++;
}
//
// scia_fifo_init - Initialize the SCI FIFO
//
void scia_fifo_init()
{
    SciaRegs.SCIFFTX.all = 0xE040;  //clear interrupt flag, re-enable operation, enable enhancements, resume operation for auto-baud
    SciaRegs.SCIFFRX.all = 0x2044;  //clear interrupt flag, re-enable operation, interrupt level
    SciaRegs.SCIFFCT.all = 0x0;
    ScibRegs.SCIFFTX.all = 0xE040;
    ScibRegs.SCIFFRX.all = 0x2044;
    ScibRegs.SCIFFCT.all = 0x0;
}
//
// End of file
//