This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD28035ISO: Failed connect to CCS debug if connect two USB to one same PC

Part Number: TMDSCNCD28035ISO


Hi,

TMDSCNCD28035ISO control card + Docking Station.

It's failed to connect with CCS debug when connect below USB A and USB B to one PC.

But it can connect to CCS debug if connect USB A and USB B to two PC separately. Why?

  • Hi Daniel,

    Since both USBs connect up to an xds100v2 emulator, CCS & the computer can sometimes get confused about which xds100v2 to use.

    Could you please add a jumper to position J8 on the Docking Station baseboard? 
    (this will put the xds100v2 that isn't being used into reset)

    Hopefully this resolves the issue.


    Thank you,
    Brett