Other Parts Discussed in Thread: CCSTUDIO, MOTORWARE
Tool/software: TI C / C ++ 컴파일러
Hello Dear friends,
I recently bought the product about TMDSHVMTRPFCKIT and F2806x controlCard and PMSM,BLDC MOTOR..
but, It is suffering because it has not been implemented..
The error details are as follows.
Restarting Program Model...
Initializing target : D:\guicomposer\webapps\InstaSPIN_FOC_F2806xM\appConfig.ccxml
Connecting target: Texas Instruments XDS100v2 USB Emulator_0/C28xx
sun.org.mozilla.javascript.internal.WrappedException: Wrapped com.ti.ccstudio.scripting.environment.ScriptingException: Error connecting to the target: emulation failure occurred (<Unknown source>#14) in <Unknown source> at line number 14Restart Completed.
I used the following program.
(InstaSPIN_FOC_F2806xM)
However, it does not continue to run with the same error.
I'll attach the picture that I've compiled on the kit.
Please help me.
I unfortunately burned the same product kit. because It's the wrong way to connect..
Please help me. thank you..