This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28027F: How do we know that the Identification values are correct?

Part Number: TMS320F28027F

Hi everyone!

Good day!

recently I identified 5Kw motor ,the values of Ls_d ,Ls_q seem to be incorrect!

the values are just like this:

Pols= 2
Rr=(0.668844)
Rs=(0.963945)
Lsd= 0.000363
Lsq= 0.000363
FluxRate = 6.26
MagCurrent =5.3
ResCurr =5.2
Max Current =11

maybe you are wondering why I used the ResCurr =5.2A ,the answer is  ,because less than that Ls became equal to Zero look like this Lsd= 0.00000.

anyway,It seems to me that  the Lsd= 0.000363 and Lsq= 0.000363 values are Too low !

so the questions here are:

1. what is the limitation for Ls_d and Ls_q for 5kw motor?

2.In which condition we are supposed to set Ls_d equal to Ls_q?

thanks for your attention

Regards.

Dave.