This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28075: Total Power Dissipation and Maximum Case Temperature

Part Number: TMS320F28075


Hi E2E,

Good day.

Our customer is looking for the Total Power Dissipation (Pd) and Maximum Case Temperature (Tcmax) of TMS320F28075PZPT. This information is not in the datasheet, is there a way to compute these parameters?

Thank you in advance for your help.

Regards,
Carlo

  • Hi Carlo,

    Please refer to "Table 5-1. Device Current Consumption at 120-MHz SYSCLK" (Operational current) to compute Total Power Dissipation based on the Supply voltage.

    We do not specify Maximum Case Temperature, but that can be calculated using the link to Application note below the datasheet table "5.1 Absolute Maximum Ratings" (foot note 3).

    Regards,

    Nirav