Part Number: TMS320F28379S
Other Parts Discussed in Thread: OPA320, REF6033, REF3433
Hi,
We're using the 28379S in motor control application.
we use Vrefhi @ 3V with REF5030AIDR (powered from 5V) followed by OPA320 (powered from 3.3V). output series cap and resistor is 560mOhm and 2.2uF.
each ADC Vrefhi has it's own OPA320.
All the analog signals go through a unity-gain buffer before connected to the ADC pins.
we're using the buffer TLV9064IDR. output capacitor between TLV9064IDR and ADC pin set to 22pF.
the question is what voltage should we supply the buffer?
we think the reasonable answer would be the 3V ref.
however in all the designs we saw the buffer is connected to the 3.3V. so maybe another consideration?
thanks a lot and appreciate also comments about the Vref circuit.