Part Number: AMIC110
Other Parts Discussed in Thread: C2000WARE
Hello
Currently, we have a drive using the Ti F28377 processor. (Based on the IDDK demo board)
This drive implement de DS402 with CAN and EtherCAT via Beckoff ET1100 linked to the Cpu on SPI (Use Ecat stack SSC)
Now, we would add PROFINET protocol.
To do this, I seen PRU-ICSS-PROFINET-SLAVE that we could place into SITRA AMIC110 with an RTOS.
But how is the link with the main processor F28377 (via SPI).
Is software on F28377 side exist to get some information from SITRA (Profinet network)
Is there some Exemple?
Regards