Part Number: TMDSEMU110-U
Other Parts Discussed in Thread: TMS320F28335,
Tool/software: Code Composer Studio
Hello,
I recently purchased the TMDSEMU110-U USB debug probe for Debugging/ Programming an Active Front end Controller which uses a Texas Instruments TMS320F28335 DSP.
When I Connect my XDS 110 USB Debugger (TMDSEMU110-U) to the JTAG Terminal of the Board, The USB probe is not visible/detected in CCS V9 as well as the Windows Device Manager.
Only the GREEN LED of the TMDSEMU110-U glows when connected to the PC Via USB.
I have tried using different USB Cables and also tried to connect the USB probe in CCS V9 using LInux OS (Xubuntu 18.04) but the TMDSEMU110-U is not being detected there as well.
Please Assist.
Regards,
Meenakshi