Hello forum!
I use the dsp2802x_epwm.h header file and there the EPWM_REGS structure according to the TI cookbook :)
When using a struct pointer with this structure a pointer++ will fail to hit the next pwm because the struct ist 6 words too short.
Proposal: add 6 extra reserved words at the end of the structure like in the structure and the pointer construct will work.
I tested it and it works but I'm courious whether that would be worth to update it into the next release of the header files.
regards
FJ